Acquia Team testing14 Skip to main content
Logo print

Legrand in the fast lane with Birmingham box project | Legrand United Kingdom

 

 

Legrand in the fast lane with Birmingham box project

Legrand’s Swifts perforated cable tray has been used for new overhead gantries currently being installed as part of the Birmingham Box M6 upgrade project. It is aimed at relieving congestion on this notoriously busy stretch of road by using technology to enforce variable speed limits, and enabling the hard shoulder to be opened up as a running lane during peak times.

I had no hesitation in using Legrand’s high quality heavy duty cable tray system. It has consistently been on time and budget with previous major contracts

Clive Brooker
Company Buyer at Nusteel

Swift perforated cable tray, Birmingham box m6, cable management case study

 Birmingham, United Kingdom - April 2013

Legrand’s Swifts perforated cable tray has been used for new overhead gantries currently being installed as part of the Birmingham Box M6 upgrade project.

Work on the project, which will make the M6 a managed motorway between junction 5 and 8, began in April 2012 and is due for completion in 2014. It is aimed at relieving congestion on this notoriously busy stretch of road by using technology to enforce variable speed limits, and enabling the hard shoulder to be opened up as a running lane during peak times.

The overhead gantries, which will house CCTV and signalling equipment, are being installed by Nusteel. The Kent-based steel bridge and gantry specialist chose to specify Swifts SRF heavy duty cable tray following the completion of similar successful projects on the M1 and M25.

Clive Brooker, company buyer at Nusteel, said: “I had no hesitation in using Legrand’s high quality heavy duty cable tray system. It has consistently been on time and budget with previous major contracts.”

Swifts perforated cable tray is available in four types, from light duty through to extra heavy duty return flange,  each of which are supported by a fully integrated range of time-saving fixings and fittings that reduce installation time and cost. These include an integral coupler system on all fittings, unique adjustable bends, and a quick-fit coupler, which is available for straight lengths on the MRF (medium duty) and SRF products.  In addition, its distinctive slot pattern provides installers with total flexibility when it comes to the positioning of nuts and bolts, cable ties and other ancillary items.

Due to the external location of the installation, the Swifts tray was specified in a hot dipped galvanised finish, which delivers excellent corrosion resistance properties.

Swifts, along with Salamandre and Cablofil, is a key brand in Legrand’s market leading UK cable management business unit

5th July 2024.9