Acquia Team testing14 Skip to main content
Logo print

Miniature detectors helps make COVID wards safer | Legrand United Kingdom

 

 

Miniature detectors helps make COVID wards safer

CP Electronics miniature presence detectors have been incorporated into a state-of-the-art disinfection device from Amity International to make hospital wards safer from COVID. Amity International is a specialist disinfectants manufacturer with an excellent reputation for product innovation, including the AIRDECON UVC which kills micro-organisms using the power of UVC light, providing fast disinfection and minimal room downtime.

By incorporating CP Electronics PIR sensors into our systems we can confidently operate these powerful systems in a busy hospital environment and have peace of mind that the staff and patients are protected from accidental UV exposure

STEPHEN BYRNE
TECHNICAL MANAGER AT AMITY INTERNATIONAL

Image of Amity international Airdecon-uvc, featuring CP Electronics PIR sensors

 Barnsley, United Kingdom - December 2021

CP Electronics miniature presence detectors have been incorporated into a state-of-the-art disinfection device from Amity International to make hospital wards safer from COVID. Amity International is a specialist disinfectants manufacturer with an excellent reputation for product innovation, including the AIRDECON UVC which kills micro-organisms using the power of UVC light, providing fast disinfection and minimal room downtime.

Amity International was looking for a sensor small enough to fit into the revolutionary AIRDECON UVC device without the need for any changes to the design. CP Electronics advised Amity that the EBMHS miniature presence detectors would be perfect for their requirements due not only to their compact proportions but also their superior detection performance. The sensors provide occupancy status as an open-collector switching output and provide an excellent detection range of up to 7m forward detection and up to 8m each way.

To ensure the safety of patients and staff within the hospital, the device is installed with four CP Electronics mini presence detectors that shut down the UVC emissions if any movement is detected. A light and buzzer give further signals to ensure the occupant is aware that the UVC device is deployed in the room. The use of CP Electronics occupancy sensors allows this powerful device to do its job safely and reliably and by accurately detecting any human presence, the possibility of human exposure to harmful UV emissions is minimised.

Stephen Byrne, Technical Manager at Amity commented “By incorporating CP Electronics PIR sensors into our AIRDECON UVC systems we can confidently operate these powerful systems in a busy hospital environment and have peace of mind that the staff and patients are protected from accidental UV exposure.”

The AIRDECON UVC fitted with CP Electronics PIR sensors can be seen at this address https://www.amityinternational.com/product/airdecon-uv-c/

5th July 2024.9